ZED Link Quad on AGX Orin

Open in ClaudeOpen in ChatGPT

This tutorial will help you set up the ZED Link Quad GMSL2 capture card, and use the StereoLabs GMSL2 cameras with the NVIDIA® Jetson™ Orin AGX Developer Kits.

Prerequisites

Make sure that you have the following items before starting this guide:

  • 1x NVIDIA® Jetson™ Orin AGX Developer Kit.
  • 1x ZED Link Quad GMSL2 capture card
  • 2x 1-to-4 GMSL2 Fakra Male to Female cables (included in the box)
  • 1x NVIDIA® power supply to power the Development Kit (included with the devkit)
  • 9V-19V (min 6W) power input (Barrel Jack 5.5 mm outer diameter, 2.5 mm inner diameter) to power the GMSL2 capture card (not included)
  • [Optional] Enclosure for Orin AGX Developer Kit
ZED Link Quad on AGX Orin materials

If you encounter any issues during the installation process, please refer to the troubleshooting page or contact support@stereolabs.com.

Install the GMSL2 Capture Card

Please make sure the DevKit and the capture card are not connected to a power source before beginning the installation process.

Plug the capture card into the ‘Camera connector’ slot and secure it using the three provided screws:

ZED Link Quad camera connector

It’s important to use the provided spacers and screws to ensure a secure fit and avoid damaging the ZED Link device and the NVIDIA® Jetson™ AGX Developer Kit carrier board. StereoLabs is not responsible for any damage caused by improper installation and will not provide support for issues arising from incorrect installation procedures.

ZED Link Quad screws installation

Connect the power adapter cable to the white J10 connector.

ZED Link Quad power connection

[Optional] AGX Orin Developer Kit Enclosure

If you are using an AGX Orin Developer Kit, we recommend you use the Enclosure for the AGX Orin Developer Kit available for purchase on the StereoLabs store, to securely integrate our GMSL2 Capture Card while keeping the electronics safe. It also allows you to mount the Dev Kit on any surface using VESA 75x75, and gives the possibility to add WiFi antennas to boost your AGX Orin wireless transmissions.

AGX Orin with enclosure

Remove the 4 screws under the AGX Orin, and remove the factory enclosure.

With the capture card already installed (as shown above) on the Dev Kit, place the enclosure and screw it in as shown below:

AGX Orin enclosure installation

Connect the camera

Connect one of the 8 wires from the female end of the two GMSL2 1-to-4 Fakra cables to your GMSL2 camera. When you hear a click, the cable is securely connected to the camera.

ZED X with Fakra cable

Ideally, GMSL2 cameras should be plugged in before booting up. If this is not the case, you can restart the zed_x_daemon that will be installed by the driver in the next section.

Once the cables are connected, plug the power for the GMSL2 capture card (9V-19V) so that cameras will be powered through the FAKRA cable (PoC).

Power adapter connection

Then connect optional HDMI/Keyboard/Mouse to USB and the power. Wait for boot up.

Now that the Developer Kit has been correctly set up, we can install the associated software and drivers for the ZED GMSL2 cameras.

Setting up the software

After setting up your ZED Link GMSL2 capture card, please follow this guide to Install the ZED Link Driver.

Install the ZED SDK

After installing the ZED Link driver, please follow this guide to Install the ZED SDK on NVIDIA® Jetson.

Multi-camera configurations

The ZED Link Quad provides 8 GMSL2 ports organized in 6 Groups (A, B, C, D, E, F):

  • Group A: port #0
  • Group B: port #1
  • Group C: port #2
  • Group D: port #3
  • Group E: ports #4 and #5
  • Group F: ports #6 and #7
ZED Link Quad connections

Please refer to the table below to understand how different camera configurations provide different image capture behaviors, according to the number of cameras, their type, and the Group they are connected to:

Camera TypeCamera ModelMax number of cameras
per Group
Max Resolution/FPS
per Group
MonocularZED X One GS
ZED X One S
Up to 2 camerasHD1200@60fps
HD1080@60fps
SVGA@120fps
MonocularZED X One 4k1 camera
only to port #0, #2, #4, #6
4k@15fps
HD1080@60fps
SVGA@60fps
StereoZED X
ZED X Mini
ZED X Nano
1 CameraHD1200@60fps
HD1080@60fps
SVGA@120fps
StereoZED X
ZED X Mini
ZED X Nano
Up to 2 CamerasHD1200@30fps
HD1080@30fps
SVGA@60fps
MixedZED X One GS/ZED X One S
+
ZED X/ZED X Mini/ZED X Nano
1 ZED X One GS/S + 1 ZED X/MiniHD1200@60fps
HD1080@60fps
SVGA@120fps

Maximum resolution and framerate require no more than 2 cameras per 4-wire GMSL2 Fakra connector.

Enable full onboard synchronization

The ZED Link Quad card is essentially a composition of two ZED Link Duo cards. By default, the two GMSL2 deserializers on the card are not synchronized together, causing the cameras connected to one 4-wire GMSL2 Fakra connector to have different capture timestamps from the cameras connected to the second 4-wire GMSL2 Fakra connector. To enable full synchronization, you must follow this procedure:

  • Open a terminal (Ctrl+Alt+T)

  • Edit the zed_x_daemon service file:

    sudo nano /etc/systemd/system/zed_x_daemon.service
    • Search for sync_mode=<x> and change it to sync_mode=1
    • Save the file and exit (Ctrl+X, Y, Enter)
  • Instruct systemd to reload all service files and update its internal configuration

    sudo systemctl daemon-reload
  • Connect the pin #13 to the pin #16 of the synchronization connector.

    Unfortunately, the pins are not aligned, so you cannot use a jumper but you can use a small wire to connect the two pins together.

    ZED Link Quad J17 sync connector

    It’s not required to connect the GND pins together as they are already connected internally on the board.

  • Restart the zed_x_daemon service

    sudo systemctl restart zed_x_daemon.service

Now, all the cameras connected to the ZED Link Quad will have synchronized frame acquisition with 15µs precision.

Although frames are hardware-synchronized with 15µs precision, software timestamps are assigned upon driver receipt and may exhibit slight millisecond-level jitter. Frames are considered synchronized if the timestamp difference is less than one frame period (1000/FPS ms).


🎉 Congratulations! You have successfully set up your StereoLabs GMSL2 Capture Card and started exploring its features. Now that you have the camera up and running, it is time to start experimenting and building your projects.

Whether you are using the camera for robotics, computer vision, or something else entirely, the ZED GMSL2 cameras are a powerful tool that can help you achieve your goals. Happy coding!