ROS 2 - ZED Mono Node
ROS 2 - ZED Mono Node
The easiest way to start a ZED ROS 2 node for a monocular camera is by using the command line:
where <camera model> must be replaced with one in the list zedxonegs, and zedxone4k
Published Topics
The ZED node publishes data to the following topics:
-
Image streams
The image topic names are created using the following naming convention:
~/<sensor_type>/<color_model>/<rect_type>/imageStarting from version 5.1.0 of the ROS 2 Wrapper the new convention replaces the previous formats such as
~/<sensor_type>/image_<rect_type>_<color_model>and~/<sensor_type>_<rect_type>/image_<rect_type>_<color_model>(e.g.,~/left/image_rect_color,~/rgb_raw/image_raw_gray). Please update your launch files and scripts to use the new topic names.- RGB channel
~/rgb/color/rect/image: Color rectified image.~/rgb/color/rect/camera_info: Color camera calibration data.~/rgb/gray/rect/image: Grayscale rectified image.~/rgb/gray/rect/camera_info: Grayscale camera calibration data.~/rgb/color/raw/image: Color unrectified image.~/rgb/color/raw/camera_info: Color raw calibration data.~/rgb/gray/raw/image: Grayscale unrectified image.~/rgb/gray/raw/camera_info: Grayscale raw calibration data.
- RGB channel
-
Sensors data
~/imu/data~/imu/data_raw~/temperature~/left_cam_imu_transform
Image Transport
The ROS 2 wrapper supports the stack image_transport introduced with ROS 2 Crystal Clemmys.
All the image topics are published using the image_transport::Publisher object, correctly associating the sensor_msgs::msg::CameraInfo message to the relative sensor_msg::msg::Image message and creates the relative compressed image streams.
We recommend using the standard available image transports:
raw: uncompressed imagecompressed: JPEG or PNG compressed imagetheora: Ogg Theora compressed imagecompressedDepth: depth image compressed with a lossless algorithm
For proper association between images and their corresponding camera information, the ZED ROS 2 Wrapper also publishes camera_info topics for all compressed image streams:
~/rgb/color/rect/image/camera_info~/rgb/gray/rect/image/camera_info~/rgb/color/raw/image/camera_info~/rgb/gray/raw/image/camera_info
The image transport topics are not advertised if NITROS is enabled. Please refer to the dedicated section about NVIDIA® Isaac ROS Nitros for more details.
NVIDIA® Isaac ROS Nitros
The ZED ROS 2 Wrapper supports the NVIDIA® Isaac™ ROS Nitros package for zero-copy transport of ROS messages using NVIDIA® GPUDirect® RDMA.
NVIDIA® Isaac ROS Nitros integration is enabled and used only if the required packages are manually installed. They are not added as a dependency because this is an optional feature.
For more information about the installation and usage of the NVIDIA® Isaac™ ROS packages, please refer to the dedicated section of the documentation: ZED Isaac™ ROS Integration Overview.
QoS profiles
All the topics are configured by default to use the following ROS 2 QoS profile:
- Reliability: RELIABLE
- History (Depth): KEEP_LAST (10)
- Durability: VOLATILE
- Lifespan: Infinite
- Deadline: Infinite
- Liveliness: AUTOMATIC
- Liveliness lease duration: Infinite
Read the official ROS 2 documentation about the QoS and the relatived settings for details.
The QoS settings can be modified by changing the relative parameters in the YAML files, as described in this official ROS 2 design document.
When creating a subscriber, be sure to use a compatible QOS profile according to the following tables:
Compatibility of QoS durability profiles:
Compatibility of QoS reliability profiles:
In order for a connection to be made, all of the policies that affect compatibility must be compatible. For instance, if a publisher-subscriber pair has compatible reliability QoS profiles, but incompatible durability QoS profiles, the connection will not be made.
for a detailed list of all the compatibility settings, please refer to the official ROS 2 documentation.
Configuration parameters
Specify your launch parameters in the common_mono.yaml, zedxonegs.yaml, and zedxone4k.yaml files available in the folder zed_wrapper/config.
General parameters
Namespace: general
common_mono.yaml
* Dynamic parameter
zedxonegs.yaml, and zedxone4k.yaml
Streaming server parameters
Namespace: stream_server
common_mono.yaml
Video parameters
Namespace: video
common_mono.yaml
* Dynamic parameter
zedxone4k.yaml
Sensors parameters
Namespace: sensors
common_mono.yaml
* Dynamic parameter
Debug parameters
Namespace: debug
common_mono.yaml
Dynamic parameters
The ZED node lets you reconfigure many parameters dynamically during the execution of the node. All the dynamic parameters are indicated with a * in the list above and with the tag [DYNAMIC] in the comments of the YAML files.
You can set the parameters using the CLI command ros2 param set, e.g.:
if the parameter is set successfully, you will get a confirmation message:
In the case you tried to set a parameter that’s not dynamically reconfigurable, or you specified an invalid value, you will get this type of error:
and the ZED node will report a warning message explaining the error type:
You can also use the Configuration -> Dynamic Reconfigure plugin of the rqt tool to dynamically set parameters by using a graphic interface.

Transform frames
The ZED ROS 2 wrapper broadcasts multiple coordinate frames that each provides information about the camera’s position and orientation. If needed, the reference frames can be changed in the launch file.
<camera_name>_camera_linkis the current position and orientation of the ZED base center. It corresponds to the bottom central fixing hole.<camera_name>_camera_centeris the current position and orientation of ZED middle baseline, determined by visual odometry and the tracking module.<camera_name>_camera_frameis the position and orientation of the ZED’s CMOS sensor.<camera_name>_camera_opticalis the position and orientation of the ZED’s camera optical frame.<camera_name>_imu_linkis the origin of the inertial data frame (not available with ZED).

Services
The ZED node provides the following services:
~/enable_streaming: enable/disable a local streaming server.
Services can be called using the rqt graphical tool by enabling the plugin Plugins -> Services -> Service caller.
It is possible to call a service also by using the CLI command ros2 service call.
For example to start Object Detection for the ZED2 camera:
and the service server will reply:
Assigning a GPU to a camera
To improve performance, you can specify the gpu_id of the graphic card that will be used for the depth computation in the common_mono.yaml configuration file. The default value (-1) will select the GPU with the highest number of CUDA cores. When using multiple ZEDs, you can assign each camera to a GPU to increase performance.