ZED Isaac™ Sim Extension Overview

Open in ClaudeOpen in ChatGPT

Build, test, and train your physical AI before the hardware even exists.

The ZED Camera extension brings faithful digital twins of every ZED camera into NVIDIA® Isaac™ Sim’s photorealistic simulation. Your simulated ZED streams data to the ZED SDK exactly like a real camera would, so the exact software you ship (perception, navigation, your ROS 2 stack) runs unchanged against the simulator. Iterate on your robot in a fully repeatable virtual world, then deploy to the field with confidence.

image

What you get:

  • ✅ Every ZED camera as a calibrated digital twin: stereo and mono models, with their lens variants
  • ✅ Stereo images + IMU streamed to the ZED SDK and ZED ROS 2 Wrapper, with zero code change
  • Ground-truth depth streaming, straight into your ZED SDK pipeline
  • ZED Sim2Real, a realistic camera model that adds real-world imaging on top of the clean render (experimental)
  • ✅ ZED observations as GPU tensors in Isaac™ Lab, for reinforcement & imitation learning
  • SDK-free RGB + depth capture for quick synthetic datasets
  • Multi-camera streaming: several cameras on one robot or a whole fleet in one scene, stereo and mono mixed, all streaming simultaneously
  • ✅ Low-latency IPC streaming and virtual stereo pairs

Why simulate your ZED?

ZED Sim2Real comparison

Left: real ZED X. Middle: raw Isaac™ Sim render. Right: the same render with the ZED Sim2Real model applied.

Choosing a data path

Whatever your workflow (sim-to-real validation, robot learning, or dataset generation), there is a data path for it:

Only the streaming path involves the ZED SDK and its stereo-matched depth; the other two deliver Isaac™ Sim’s ground-truth renderer depth.

Get started

Get your first simulated ZED streaming in a few steps: install Isaac™ Sim, the ZED SDK, and the ZED Camera extension, then drop a ZED into your scene and press Play.

This is documentation for the ZED Camera extension >= 5.0.0, which targets NVIDIA® Isaac™ Sim 6.0 (Kit 110.1.2). Extension 4.x targets Isaac™ Sim 5.0, 3.x targets 4.5, and 2.x targets 4.0; see the compatibility table.

You can find the documentation for older versions here.