ZED Link Duo on Xavier NX

Open in ClaudeOpen in ChatGPT

This tutorial will help you set up the ZED Link Duo GMSL2 capture card, and use the StereoLabs GMSL2 cameras with the NVIDIA® Jetson™ Xavier NX Developer Kits.

Prerequisites

Make sure that you have the following items before starting this guide:

  • 1x NVIDIA® Jetson™ Xavier NX Developer Kit.
  • 1x ZED Link Duo GMSL2 capture card
  • 1x 1-to-4 GMSL2 Fakra Male to Female cable (included in the box)
  • 1x NVIDIA® power supply to power the Development Kit (included with the devkit)
  • 2x FPC Camera Cable 15-pin 1.0mm (not included)*
  • 9V-19V (min 2W) power input (Barrel Jack 5.5 mm outer diameter, 2.5 mm inner diameter) to power the GMSL2 capture card (not included)

The 15-pin CSI cable must not be mistaken for a DSI cable, where the active pin connection is on the same side. On CSI, the 15 pins are on the opposite side when looking at the flat cable. The cable can be purchased at UCTRONICS.

MIPI cables carry high-speed video signals, and longer cables can introduce noise or signal degradation. For optimal performance, use cables no longer than 15 cm.

Xavier NX material

If you encounter any issues during the installation process, please refer to the troubleshooting page or contact support@stereolabs.com.

Install the GMSL2 Capture Card

Please make sure the DevKit and the capture card are not connected to a power source before beginning the installation process.

Cabling the GMSL2 Capture Card

Connect the CSI cable at each MIPI 15-pin port of the carrier board. Make sure the correct side is plugged in for each port.

Xavier NX capture card cabling

Inverting the side might damage the carrier board or the capture card.

Both MIPI cables must be connected to have access to 2x ZED GMSL2 cameras on the capture card.

Cabling the Carrier Board

Connect the CSI cable to the carrier board 22-pin connector.

Make sure that J9/CAM0 is connected to the centered MIPI port of the GMSL2 capture card.

J1/CAM1 must be connected to the MIPI port close to the edge.

Make sure to respect the side of the MIPI pins, according to the following picture:

Xavier NX capture card cabling orientation

Once connected, the setup should look like the following picture:

Xavier NX cabled

Connect the camera

Connect the GMSL2 Fakra cable female end to your ZED X. When you hear a click, the cable is securely connected to the camera.

ZED X with Fakra cable

With the capture card still powered off, connect the male end of the cable to the capture card’s GMSL2 input. Again, a click informs you that the cable is secured.

Ideally, GMSL2 cameras should be plugged in before booting up. If this is not the case, you can restart the zed_x_daemon that will be installed by the driver in the next section.

Xavier NX plug camera

Once the cables are connected, plug the power for the GMSL2 capture card (9V-19V) so that cameras will be powered through the FAKRA cable (PoC).

Then connect optional HDMI/Keyboard/Mouse to USB and the power. Wait for boot up.

Now that the Developer Kit has been correctly set up, we can install the associated software and drivers for the ZED GMSL2 cameras.

Setting up the software

After setting up your ZED Link GMSL2 capture card, please follow this guide to Install the ZED Link Driver.

Install the ZED SDK

After installing the ZED Link driver, please follow this guide to Install the ZED SDK on NVIDIA® Jetson.

Multi-camera configurations

The ZED Link Duo provides 4 GMSL2 ports organized in 2 Groups (A, B):

  • Group A: port #0 and port #1
  • Group B: port #2 and port #3
ZED Link Duo connections

Please refer to the table below to understand how different camera configurations provide different image capture behaviors, according to the number of cameras, their type, and the Group they are connected to:

Camera TypeCamera ModelMax number of cameras
per Group
Max Resolution/FPS
per Group
MonocularZED X One GS
ZED X One S
Up to 2 camerasHD1200@60fps
HD1080@60fps
SVGA@120fps
MonocularZED X One 4k1 camera
only to port #0, #2
4k@15fps
HD1080@60fps
SVGA@60fps
StereoZED X
ZED X Mini
ZED X Nano
1 CameraHD1200@60fps
HD1080@60fps
SVGA@120fps
StereoZED X
ZED X Mini
ZED X Nano
Up to 2 CamerasHD1200@30fps
HD1080@30fps
SVGA@60fps

Maximum resolution and framerate require no more than 2 cameras per 4-wire GMSL2 Fakra connector.


🎉 Congratulations! You have successfully set up your StereoLabs GMSL2 Capture Card and started exploring its features. Now that you have the camera up and running, it is time to start experimenting and building your projects.

Whether you are using the camera for robotics, computer vision, or something else entirely, the ZED GMSL2 cameras are a powerful tool that can help you achieve your goals. Happy coding!