Flash your ZED Box Mini
Should I flash my ZED Box Mini? #
The ZED Box Mini is shipped with a pre-configured operating system and drivers optimized for its hardware.
Flashing (resetting or upgrading the device firmware) is only recommended if you need to:
- Install a different OS or JetPack version,
- Recover from a corrupted system,
- Resolve issues preventing the device from booting or functioning properly.
⚠️ Caution: Flashing will erase all data and custom configurations on your ZED Box Mini. Proceed only if you are familiar with the process or have been instructed by support. For most users, flashing should be a last resort.
Flashing Procedure #
⚠️ The NVIDIA® SDK Manager does not support automatic flashing of the Jetson modules installed in the ZED Box. Therefore, you must manually flash the board using NVIDIA’s BSP for the desired JetPack version.
Force the ZED Box Mini in Recovery mode #
⚠️ It is not required to open the ZED Box Mini to force it into Recovery mode. Opening the box will void the warranty ⚠️
First method:
Note: This is applicable only if your device can normally boot.
Open a terminal console (
Ctrl+Alt+t) and enter the commandsudo reboot --force forced-recoverySecond method:
- Connect the power
- Use a pin to push the
RCVbutton - While keeping the
RCVbutton pushed, use a pin to push theRSTbutton
Check that the ZED Box Mini restarted in Force Recovery mode #
Connect a Type-A/MicroUSB cable to a host device running Ubuntu 22.04 and to the OTG port of the ZED Box Mini.
Open a terminal console (Ctrl+Alt+t).
You can verify that the ZED Box Mini correctly started in “Recovery Mode” by entering this command:
lsusb -d '0955:'
- NVIDIA® Jetson™ Orin Nano 4 GB: an NVIDIA® device with VID:PID
0955:7623should be listed. e.g.Bus xxx Device yyy: ID 0955:7623 NVIDIA Corp. APX - NVIDIA® Jetson™ Orin Nano 4 GB: an NVIDIA® device with VID:PID
0955:7523should be listed. e.g.Bus xxx Device yyy: ID 0955:7523 NVIDIA Corp. APX - NVIDIA® Jetson™ Orin NX 8 GB: an NVIDIA® device with VID:PID
0955:7423should be listed. e.g.Bus xxx Device yyy: ID 0955:7423 NVIDIA Corp. APX - NVIDIA® Jetson™ Orin NX 16 GB: an NVIDIA® device with VID:PID
0955:7323should be listed. e.g.Bus xxx Device yyy: ID 0955:7323 NVIDIA Corp. APX
📌 Note: If an NVIDIA® device with VID:PID
0955:7020and typeNVIDIA Corp. L4T (Linux for Tegra) running on Tegrais listed, then your ZED Box Mini has not rebooted in Force Recovery mode. You must retry the procedure.
Flash the ZED Box Mini #
Requirements:
- use a host PC running Ubuntu 20.04 or Ubuntu 22.04.
⚠️ Warning: do not use virtual machines or WSL2 to run Ubuntu to flash the ZED Box Mini. If you do not have a ready PC running Ubuntu, please consider using a Live USBKey instead:
On the host PC:
Open a terminal console from an empty folder of your choice.
For example:
mkdir -p ~/zedbox_flash cd ~/zedbox_flash
Ensure that you previously booted the ZED Box Mini in “Recovery mode”.
Download the Flash Script:
- Download the flash script for the NVIDIA® Jetpack version you want to install:
Flash the ZED Box Mini:
- Ensure you have at least 80GB of free space on your working hard drive.
- Use the following command to flash the ZED Box:
Standard mode:
BSP_ROOT=./stereolabs_bsp/ ./zedbox_<version>.sh`Super mode - ⚠️ This mode requires the fan to be installed ⚠️
BSP_ROOT=./stereolabs_bsp/ PWR_MODE=SUPER ./zedbox_<version>.sh`
Replace
<version>with the installer name, e.g.,zedbox_all_usb_flash_6.2.sh.All necessary files will be downloaded in the folder
$BSP_ROOT. The script will create this folder if it does not exist and will ask you to log in asroot.Wait for the operation to complete. You will see the following output if the flash is successful:
[...] Flash is successful Reboot device Cleaning up... Log is saved to Linux_for_Tegra/initrdlog/flash_<bla_bla_bla>.log FLASH SUCCESS
If you encounter any problems during this procedure, please consult the troubleshooting guide.
Post-Flash operations #
After flashing your device, follow these steps to install the necessary NVIDIA® and Stereolabs packages to ensure your ZED camera works correctly.
Boot and Login:
- Power on the device and log in with your credentials.
The new default credentials of your ZED Box are:
- username:
user - password:
admin
Check the OS Version:
- Follow this support guide to determine the version of the operating system installed on your device.
Connect to the Internet:
- Connect your device to the internet using an Ethernet cable or WiFi.
Open a Terminal:
- Press
Ctrl+Alt+Tto open a terminal window.
- Press
Update the System:
- Run the following commands to update your system packages:
sudo apt update sudo apt upgrade -y📌 Note: if you get this error after
sudo apt upgrade -y:[...] Errors were encountered while processing: nvidia-l4t-bootloader nvidia-l4t-kernel nvidia-l4t-kernel-headers nvidia-l4t-jetson-io nvidia-l4t-kernel-oot-modules nvidia-l4t-display-kernel nvidia-l4t-kernel-oot-headers nvidia-l4t-kernel-dtbs E: Sub-process /usr/bin/dpkg returned an error code (1)You can fix it by running these commands:
sudo apt-get autoclean # Clean up the package cache sudo mv /var/lib/dpkg/info/ /var/lib/dpkg/backup/ # Backup the info directory sudo mkdir /var/lib/dpkg/info/ # Create a new info directory sudo apt-get update # Update the package list sudo apt-get -f install # Fix broken dependenciesThis process will clean up the package cache, backup the existing package information, create a new directory for package information, update the package list, and fix any broken dependencies that may be causing the issue.
Install NVIDIA® Jetpack Packages:
- Run the following command to install the NVIDIA® Jetpack packages, which include the required Jetson™ drivers, CUDA, and all necessary NVIDIA® libraries:
sudo apt install nvidia-jetpackDownload the ZED SDK:
- Visit the Stereolabs website and download the ZED SDK for Jetson that matches your installed Jetpack/L4T version.
Install the ZED SDK:
Navigate to your Downloads directory and run the installer:
cd ~/Downloads chmod +x ZED_SDK_Tegra_L4T_v<x.y.z>.zstd.run ./ZED_SDK_Tegra_L4T_v<x.y.z>.zstd.run
Install ZED Link Drivers (for ZED X or ZED X One Cameras):
Download and install the appropriate drivers from the driver web page:
cd ~/Downloads sudo dpkg -i stereolabs-zedbox-mini_<ver_info>.sh
Reboot:
- Restart your device to apply all changes:
sudo rebootEnjoy Your Device:
- Your device is now ready for use with the ZED cameras.