|
| struct | CalibrationParameters |
| | Intrinsic and Extrinsic parameters of the camera (translation and rotation). More...
|
| |
| class | Camera |
| | This class is the main interface with the camera and the SDK features, suche as: video, depth, tracking, mapping, and more.
Find more information in the detailed description below.
. More...
|
| |
| struct | CameraInformation |
| | Structure containing information of a signle camera (serial number, model, calibration, etc.) More...
|
| |
| struct | CameraParameters |
| | Intrinsic parameters of a camera. More...
|
| |
| class | Chunk |
| | Represents a sub-mesh, it contains local vertices and triangles. More...
|
| |
| struct | DeviceProperties |
| | Properties of a camera. More...
|
| |
| class | FusedPointCloud |
| | A fused point cloud contains both geometric and color data of the scene captured by spatial mapping. More...
|
| |
| class | IMUData |
| | Contains inertial positional tracking data which gives the orientation of the ZED-M. More...
|
| |
| class | InitParameters |
| | Holds the options used to initialize the Camera object.
Once passed to the Camera::open() function, these settings will be set for the entire execution life time of the Camera.
You can get further information in the detailed description bellow.
. More...
|
| |
| class | InputType |
| | Defines the input type used in the ZED SDK. Can be used to select a specific camera with ID or serial number, or a svo file. More...
|
| |
| class | Mat |
| | The Mat class can handle multiple matrix format from 1 to 4 channels, with different value types (float or uchar), and can be stored CPU and/or GPU side. More...
|
| |
| class | Matrix3f |
| | Represents a generic 3*3 matrix. More...
|
| |
| class | Matrix4f |
| | Represents a generic 4*4 matrix. More...
|
| |
| class | Mesh |
| | A mesh contains the geometric (and optionally texture) data of the scene captured by spatial mapping. More...
|
| |
| class | MeshFilterParameters |
| | Defines the behavior of the sl::Mesh::filter function. More...
|
| |
| class | Orientation |
| | Designed to contain orientation (quaternion) data of the positional tracking. More...
|
| |
| class | Plane |
| | A plane defined by a point and a normal, or a plane equation Other elements can be extracted such as the mesh, the 3D bounds... More...
|
| |
| class | PointCloudChunk |
| | Represents a sub fused point cloud, it contains local vertices and colors. More...
|
| |
| class | Pose |
| | Contains positional tracking data which gives the position and orientation of the ZED in 3D space. More...
|
| |
| struct | RecordingState |
| | Recording structure that contains information about SVO. More...
|
| |
| struct | Resolution |
| | Width and height of an array. More...
|
| |
| class | Rotation |
| | Designed to contain rotation data of the positional tracking. It inherits from the generic Matrix3f. More...
|
| |
| class | RuntimeParameters |
| | Parameters that defines the behavior of the grab. More...
|
| |
| class | SpatialMappingParameters |
| | Sets the spatial mapping parameters. More...
|
| |
| class | StreamingParameters |
| | Sets the streaming parameters. More...
|
| |
| struct | StreamingProperties |
| | Properties of a all streaming devices. More...
|
| |
| class | String |
| | Defines a string. More...
|
| |
| class | Texture |
| | Contains information about texture image associated to a Mesh. More...
|
| |
| class | TrackingParameters |
| | Parameters for positional tracking initialization. More...
|
| |
| class | Transform |
| | Designed to contain translation and rotation data of the positional tracking. More...
|
| |
| class | Translation |
| | Designed to contain translation data of the positional tracking. More...
|
| |
| class | Vector2 |
| | Represents a two dimensions vector for both CPU and GPU. More...
|
| |
| class | Vector3 |
| | Represents a three dimensions vector for both CPU and GPU. More...
|
| |
| class | Vector4 |
| | Represents a four dimensions vector for both CPU and GPU. More...
|
| |
|
| String | toString (const UNIT &unit) |
| | Converts the given enum to a readable string. More...
|
| |
| String | toString (const COORDINATE_SYSTEM &coord_system) |
| | Converts the given enum to a readable string. More...
|
| |
| String | toString (const ERROR_CODE &errorCode) |
| | Converts the given enum to a readable string. More...
|
| |
| String | toVerbose (const ERROR_CODE &errorCode) |
| | Return a text explaining how to fix the given ERROR_CODE. More...
|
| |
| String | toString (const MODEL &model) |
| | Converts the given enum to a readable string. More...
|
| |
| String | toString (const INPUT_TYPE &input_type) |
| | Converts the given enum to a readable string. More...
|
| |
| String | toString (const CAMERA_STATE &camera_state) |
| | Converts the given enum to a readable string. More...
|
| |
| String | toString (const DeviceProperties &properties) |
| | Converts the given struct to a readable string. More...
|
| |
| String | toString (const StreamingProperties &properties) |
| | Converts the given struct to a readable string. More...
|
| |
| void | sleep_ms (int time) |
| | Tells the program to wait for x ms. More...
|
| |
| void | sleep_us (int time) |
| | Tells the program to wait for x us. More...
|
| |
| String | toString (const MESH_FILE_FORMAT &mesh_frmt) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const MESH_TEXTURE_FORMAT &text_frmt) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const MeshFilterParameters::MESH_FILTER &mesh_filter) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const PLANE_TYPE &type) |
| | Converts the given enumerated value into readable text. More...
|
| |
| bool | saveDepthAs (Camera &zed, DEPTH_FORMAT format, String name, float factor=1.) |
| | Writes the current depth map into a file. More...
|
| |
| bool | saveDepthAs (Mat &depth, DEPTH_FORMAT format, String name, float factor=1.) |
| | Writes the current depth map into a file. More...
|
| |
| bool | savePointCloudAs (Camera &zed, POINT_CLOUD_FORMAT format, String name, bool with_color=false) |
| | Writes the current point cloud into a file. More...
|
| |
| bool | savePointCloudAs (Mat &cloud, POINT_CLOUD_FORMAT format, String name, bool with_color=false) |
| | Writes the current point cloud into a file. More...
|
| |
| String | toString (const SpatialMappingParameters::MAPPING_RESOLUTION &resolution) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const SpatialMappingParameters::MAPPING_RANGE &range) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const SpatialMappingParameters::SPATIAL_MAP_TYPE &map_type) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const MEM &mem) |
| | Convert the given enumerated value into readable text. More...
|
| |
| String | toString (const COPY_TYPE &cpy) |
| | Convert the given enumerated value into readable text. More...
|
| |
| String | toString (const MAT_TYPE &type) |
| | Convert the given enumerated value into readable text. More...
|
| |
| Rotation | computeRotationMatrixFromGravity (sl::float3 axis_to_align, sl::float3 gravity_vector) |
| | Compute the rotation matrix from the gravity vector : the rotation can used to find the world rotation from the gravity of an IMU. More...
|
| |
| Matrix3f | getCoordinateTransformConversion3f (COORDINATE_SYSTEM coord_system_src, COORDINATE_SYSTEM coord_system_dst) |
| | Get the coordinate transform conversion matrix to change coordinate system. More...
|
| |
| Matrix4f | getCoordinateTransformConversion4f (COORDINATE_SYSTEM coord_system_src, COORDINATE_SYSTEM coord_system_dst) |
| | Get the coordinate transform conversion matrix to change coordinate system. More...
|
| |
| ERROR_CODE | convertCoordinateSystem (Mat &floatMat, COORDINATE_SYSTEM coord_system_src, COORDINATE_SYSTEM coord_system_dst, MEM mem=MEM_CPU) |
| | Change the coordinate system of a matrix. More...
|
| |
| ERROR_CODE | convertCoordinateSystem (Transform &motionMat, COORDINATE_SYSTEM coord_system_src, COORDINATE_SYSTEM coord_system_dst) |
| | Change the coordinate system of a transform matrix. More...
|
| |
| float | getUnitScale (UNIT unit_src, UNIT unit_dst) |
| | Get the unit factor to change units. More...
|
| |
| ERROR_CODE | convertUnit (Mat &floatMat, UNIT unit_src, UNIT unit_dst, MEM mem=MEM_CPU) |
| | Change the unit of a matrix. More...
|
| |
| ERROR_CODE | convertUnit (Transform &motionMat, UNIT unit_src, UNIT unit_dst) |
| | Change the unit (of the translations) of a transform matrix. More...
|
| |
| String | toString (const RESOLUTION &resolution) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const CAMERA_SETTINGS &camSettings) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const SELF_CALIBRATION_STATE &selfCalibState) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const DEPTH_MODE &depthMode) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const SENSING_MODE &sensingMode) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const MEASURE &measure) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const VIEW &view) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const TIME_REFERENCE &time_reference) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const DEPTH_FORMAT &depth_frmt) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const POINT_CLOUD_FORMAT &pc_frmt) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const TRACKING_STATE &track_state) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const AREA_EXPORT_STATE &area_export) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const REFERENCE_FRAME &ref_frame) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const SPATIAL_MAPPING_STATE &mapping_state) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | toString (const SVO_COMPRESSION_MODE &svo_compression) |
| | Converts the given enumerated value into readable text. More...
|
| |
| String | resolution2str (RESOLUTION res) |
| | Converts the given RESOLUTION into a string. More...
|
| |
| String | statusCode2str (SELF_CALIBRATION_STATE state) |
| | Converts the given SELF_CALIBRATION_STATE into a string. More...
|
| |
| DEPTH_MODE | str2mode (String mode) |
| | Converts the given string into a DEPTH_MODE. More...
|
| |
| String | depthMode2str (DEPTH_MODE mode) |
| | Converts the given DEPTH_MODE into a string. More...
|
| |
| String | sensingMode2str (SENSING_MODE mode) |
| | Converts the given SENSING_MODE into a string. More...
|
| |
| String | trackingState2str (TRACKING_STATE state) |
| | Converts the given TRACKING_STATE into a string. More...
|
| |
| String | spatialMappingState2str (SPATIAL_MAPPING_STATE state) |
| | Converts the given SPATIAL_MAPPING_STATE into a string. More...
|
| |
|
| String | model2str (MODEL model) |
| | Converts the given MODEL into a string. More...
|
| |
| String | errorCode2str (ERROR_CODE errorCode) |
| | Converts the given ERROR_CODE into a string. More...
|
| |
| String | unit2str (UNIT unit) |
| | Converts the given UNIT into a string. More...
|
| |
| UNIT | str2unit (String unit) |
| | Converts the given string into a UNIT. More...
|
| |