Classes | |
| class | String |
| Defines a string. More... | |
| class | Matrix3f |
| Represents a generic 3*3 matrix. More... | |
| class | Matrix4f |
| Represents a generic 4*4 matrix. More... | |
| class | Vector2< T > |
| Represents a two dimensions vector for both CPU and GPU. More... | |
| class | Vector3< T > |
| Represents a three dimensions vector for both CPU and GPU. More... | |
| class | Vector4< T > |
| Represents a four dimensions vector for both CPU and GPU. More... | |
| struct | Resolution |
| Width and height of an array. More... | |
| class | Mat |
| The Mat class can handle multiple matrix format from 1 to 4 channels, with different value types (float or uchar), and can be stored CPU and/or GPU side. More... | |
Enumerations | |
| enum | MEM |
| List available memory type. More... | |
| enum | COPY_TYPE |
| List available copy operation on Mat. More... | |
| enum | MAT_TYPE |
| List available Mat formats. More... | |
Functions | |
| void | sleep_ms (int time) |
| Tells the program to wait for x ms. More... | |
| void | sleep_us (int time) |
| Tells the program to wait for x us. More... | |
| String | toString (const MEM &mem) |
| Convert the given enumerated value into readable text. More... | |
| String | toString (const COPY_TYPE &cpy) |
| Convert the given enumerated value into readable text. More... | |
| String | toString (const MAT_TYPE &type) |
| Convert the given enumerated value into readable text. More... | |
| int | getZEDSDKRuntimeVersion (int &major, int &minor, int &patch) |
| [Windows only] Returns the ZED SDK version currently installed on the computer. The major, minor, patch parameters will be filled by reference. More... | |
| const void | getZEDSDKBuildVersion (int &major, int &minor, int &patch) |
| Returns the ZED SDK version which the current program has been compiled with. The major, minor, patch parameters will be filled by reference. More... | |
| enum MEM |
| enum COPY_TYPE |
List available copy operation on Mat.
| Enumerator | |
|---|---|
| COPY_TYPE_CPU_CPU | copy data from CPU to CPU. |
| COPY_TYPE_CPU_GPU | copy data from CPU to GPU. |
| COPY_TYPE_GPU_GPU | copy data from GPU to GPU. |
| COPY_TYPE_GPU_CPU | copy data from GPU to CPU. |
| enum MAT_TYPE |
List available Mat formats.
|
inline |
Tells the program to wait for x ms.
| time | : the number of ms to wait. |
|
inline |
Tells the program to wait for x us.
| time | : the number of us to wait. |
Convert the given enumerated value into readable text.
Convert the given enumerated value into readable text.
Convert the given enumerated value into readable text.
|
inline |
[Windows only] Returns the ZED SDK version currently installed on the computer. The major, minor, patch parameters will be filled by reference.
|
inline |
Returns the ZED SDK version which the current program has been compiled with. The major, minor, patch parameters will be filled by reference.