Classes | |
| struct | RecordingStatus |
| Structure containing information about the status of the recording. More... | |
| struct | StreamingParameters |
| Structure containing the options used to stream with the ZED SDK. More... | |
| struct | RecordingParameters |
| Structure containing the options used to record. More... | |
| struct | DeviceProperties |
| Structure containing information about the properties of a camera. More... | |
| struct | StreamingProperties |
| Structure containing information about the properties of a streaming device. More... | |
| class | InitParameters |
| Class containing the options used to initialize the sl::Camera object. More... | |
| class | Camera |
| This class serves as the primary interface between the camera and the various features provided by the SDK. More... | |
| class | InitParametersOne |
| Class containing the options used to initialize the sl::CameraOne object. More... | |
Enumerations | |
| enum class | SIDE |
| Lists possible sides on which to get data from. More... | |
| enum | FLIP_MODE : int |
| Lists possible flip modes of the camera. More... | |
| enum class | RESOLUTION |
| Lists available resolutions. More... | |
| enum class | VIDEO_SETTINGS |
| Lists available camera settings for the camera (contrast, hue, saturation, gain, ...). More... | |
| enum class | VIEW |
| Lists available views. More... | |
| enum class | TIME_REFERENCE |
| Lists possible time references for timestamps or data. More... | |
| enum class | SVO_COMPRESSION_MODE |
| Lists available compression modes for SVO recording. More... | |
| enum class | MODEL |
| Lists ZED camera model. More... | |
| enum class | INPUT_TYPE |
| Lists available input types in the ZED SDK. More... | |
| enum class | CAMERA_STATE |
| Lists possible camera states. More... | |
| enum class | STREAMING_CODEC |
| Lists the different encoding types for image streaming. More... | |
| enum class | BUS_TYPE |
| Lists available LIVE input type in the ZED SDK. More... | |
| enum class | CAMERA_TYPE |
| Lists available camera types. More... | |
Functions | |
| sl::Resolution | getResolution (RESOLUTION resolution) |
| Gets the corresponding sl::Resolution from an sl::RESOLUTION. More... | |
|
strong |
| enum FLIP_MODE : int |
Lists possible flip modes of the camera.
|
strong |
Lists available resolutions.
|
strong |
Lists available camera settings for the camera (contrast, hue, saturation, gain, ...).
| Enumerator | |
|---|---|
| BRIGHTNESS | Brightness control
|
| CONTRAST | Contrast control
|
| HUE | Hue control
|
| SATURATION | Saturation control |
| SHARPNESS | Digital sharpening control |
| GAMMA | ISP gamma control |
| GAIN | Gain control
|
| EXPOSURE | Exposure control
|
| AEC_AGC | Defines if the GAIN and EXPOSURE are in automatic mode or not. |
| AEC_AGC_ROI | Defines the region of interest for automatic exposure/gain computation. |
| WHITEBALANCE_TEMPERATURE | Color temperature control
|
| WHITEBALANCE_AUTO | Defines if the white balance is in automatic mode or not. |
| LED_STATUS | Status of the front LED of the camera.
|
| EXPOSURE_TIME | Real exposure time control in microseconds.
|
| ANALOG_GAIN | Real analog gain (sensor) control in mDB.
|
| DIGITAL_GAIN | Real digital gain (ISP) as a factor.
|
| AUTO_EXPOSURE_TIME_RANGE | Range of exposure auto control in microseconds.
|
| AUTO_ANALOG_GAIN_RANGE | Range of sensor gain in automatic control.
|
| AUTO_DIGITAL_GAIN_RANGE | Range of digital ISP gain in automatic control.
|
| EXPOSURE_COMPENSATION | Exposure-target compensation made after auto exposure.
|
| DENOISING | Level of denoising applied on both left and right images.
|
|
strong |
Lists available views.
| Enumerator | |
|---|---|
| LEFT | Left (for stereo or default for monocular camera) BGRA image. Each pixel contains 4 unsigned char (B, G, R, A). |
| RIGHT | Right BGRA image. Each pixel contains 4 unsigned char (B, G, R, A). |
| LEFT_GRAY | Left gray image. Each pixel contains 1 unsigned char. |
| RIGHT_GRAY | Right gray image. Each pixel contains 1 unsigned char. |
| LEFT_UNRECTIFIED | Left BGRA unrectified image. Each pixel contains 4 unsigned char (B, G, R, A). |
| RIGHT_UNRECTIFIED | Right BGRA unrectified image. Each pixel contains 4 unsigned char (B, G, R, A). |
| LEFT_UNRECTIFIED_GRAY | Left gray unrectified image. Each pixel contains 1 unsigned char. |
| RIGHT_UNRECTIFIED_GRAY | Right gray unrectified image. Each pixel contains 1 unsigned char. |
| SIDE_BY_SIDE | Left and right image (the image width is therefore doubled). Each pixel contains 4 unsigned char (B, G, R, A). |
| DEPTH | Color rendering of the depth. Each pixel contains 4 unsigned char (B, G, R, A).
|
| CONFIDENCE | Color rendering of the depth confidence. Each pixel contains 4 unsigned char (B, G, R, A).
|
| NORMALS | Color rendering of the normals. Each pixel contains 4 unsigned char (B, G, R, A).
|
| DEPTH_RIGHT | Color rendering of the right depth mapped on right sensor. Each pixel contains 4 unsigned char (B, G, R, A).
|
| NORMALS_RIGHT | Color rendering of the normals mapped on right sensor. Each pixel contains 4 unsigned char (B, G, R, A).
|
|
strong |
|
strong |
Lists available compression modes for SVO recording.
|
strong |
Lists ZED camera model.
|
strong |
Lists available input types in the ZED SDK.
| Enumerator | |
|---|---|
| USB | USB input mode |
| SVO | SVO file input mode |
| STREAM | STREAM input mode (requires to use enableStreaming() / disableStreaming()" on the "sender" side) |
| GMSL | GMSL input mode (only on NVIDIA Jetson) |
|
strong |
|
strong |
|
strong |
|
strong |
| sl::Resolution sl::getResolution | ( | RESOLUTION | resolution | ) |
Gets the corresponding sl::Resolution from an sl::RESOLUTION.
| resolution | : The wanted sl::RESOLUTION. |