NVIDIA® has unveiled the "Super" version of the Jetson Orin Nano. Discover how to leverage the new power modes with ZED and upgrade a standard Jetson Orin Nano into a "Super" version.

The world of embedded AI computing has taken another leap forward with the introduction of the NVIDIA® Jetson Orin Nano Super. This enhanced version of the little Jetson Orin Nano Developer Kit, sold at $249, half the price from earlier, brings cutting-edge performance to AI developers and robotics enthusiasts, particularly those working with . In this blog post, we’ll explore the key features of the Jetson Orin Nano Super, how it boosts the capabilities of , and how you can upgrade your standard Orin Nano to the Super version.

Jensen Huang, NVIDIA's CEO, and founder, announced the newborn Jetson Orin Nano Developer Kit in a YouTube video unveiling it by taking it out of an oven on a tray as if it had just been baked.
The NVIDIA® Jetson Orin Nano Super with Jetpack 6.2 introduces a key enhancement: the new MAXN SUPER and 25W reference power modes. This addition provides increased computational power and flexibility, complementing the existing power modes. Here's how the modes compare:
This MAXN SUPER option is particularly beneficial for applications requiring higher performance, such as AI inference tasks, robotics, and real-time computer vision, and can be enabled on standard NVIDIA® Jetson Orin Nano Developer Kit by installing the new Jetpack 6.2.
Other relevant upgrades:
- | NVIDIA Jetson Orin Nano Developer Kit | NVIDIA Jetson Orin Nano Super Developer Kit (/w JetPack 6.2) |
GPU |
|
|
AI PERF |
|
|
CPU |
|
|
Memory |
|
|
MODULE POWER | 7W | 10W (4GB) 7W | 15W (8GB) | 10W | 25W | MAXN SUPER (4GB) |
In the upcoming section, we will compare the performance of a ZED X camera on an NVIDIA® Jetson Orin Nano running JetPack 6.0 (non Super Mode) against one running JetPack 6.2 (Super Mode), with a focus on understanding the impact of the new MAXN SUPER power mode.

We assessed the new MAXN power mode at 25W by installing JetPack 6.2 on an NVIDIA® Jetson Nano 8GB Developer Kit previously running Jetpack 6.0.
The benchmark evaluates the frequency of depth extraction for a ZED X camera at HD1200 (1900px x 1200px) resolution, utilizing a grab rate of 60 FPS. We conducted tests using classical Stereo processing in ULTRA depth mode, alongside AI-based depth extraction in both NEURAL and NEURAL+ depth modes.
A series of acquisitions were conducted on a "standard" NVIDIA® Jetson Nano 8GB devkit. Initially, the device ran Jetpack 6.0 (L4T 36.3) in 15W power mode. Subsequently, we upgraded to Jetpack 6.2 (L4T 36.4.3 GA) to enable the "Super" mode, and tested performance in both 15W and MAXN power modes.
All tests have been executed by enabling jetson_clocks to optimize CPU and GPU clock speeds.
- | ULTRA | NEURAL | NEURAL+ |
Orin Nano [15W] | 21 Hz / 16 W | 13 Hz / 18 W | 5 Hz / 20 W |
Orin Nano Super [15W] | 21 Hz / 16 W | 13 Hz / 18 W | 5 Hz / 20 W |
Orin Nano Super [MAXN] | 32 Hz / 25 W | 20 Hz / 26 W | 7 Hz / 28 W |
As expected there's no performance difference between JP6.0 and JP6.2 in 15W mode, but we see a significant boost in MAXN mode.
Please note that this boost is not limited to the GMSL2 ZED X camera; it enhances the overall performance of the ZED SDK depth processing pipeline. As a result, the USB 3 ZED 2i camera will also benefit.
All developers can achieve the "Super" performance with their NVIDIA® Jetson Orin Nano Developer Kit by either installing the latest SD Card Image that supports MAXN mode or using NVIDIA® SDK Manager.
During the installation with SDK Manager, simply select JetPack 6.2 (L4T 36.4.3 GA).

After installation, boot your device and enable MAXN mode from the power mode selector to experience the enhanced performance boost.

When your Jetson is ready you must also download and install the latest ZED X Driver (version >= 1.2.2) and the latest ZED SDK (version >= 4.2.3).
The NVIDIA® Jetson Orin Nano Super represents a significant step forward for edge AI computing, particularly in ZED camera applications. Its enhanced processing capabilities, improved memory bandwidth, and efficient power consumption make it a worthy upgrade for developers and enthusiasts looking to push the boundaries of AI and robotics. Whether you're deploying autonomous robots, smart surveillance systems, or immersive AR/VR experiences, the NVIDIA® Jetson Orin Nano Super with ZED ensures you’re equipped for the future.
Ready to leap? Upgrade your NVIDIA® Jetson Orin Nano today and unlock unparalleled performance for your ZED camera applications.