Classes | |
| struct | BatchParameters |
| Structure containing a set of parameters for batch object detection. More... | |
| struct | ObjectDetectionParameters |
| Structure containing a set of parameters for the object detection module. More... | |
| struct | ObjectDetectionRuntimeParameters |
| Structure containing a set of runtime parameters for the object detection module. More... | |
| struct | ObjectData |
| Structure containing data of a detected object such as its boundingBox, label, id and its 3D position. More... | |
| struct | CustomBoxObjectData |
| Structure that store externally detected objects. More... | |
| struct | Objects |
| Structure containing the results of the object detection module. It contains the number of object in the scene (numObject) and the objectData structure for each object. More... | |
| class | ObjectsBatch |
| Class containing batched data of a detected objects from the object detection module. More... | |
Enumerations | |
| enum class | OBJECT_CLASS |
| Lists available object classes. More... | |
| enum class | OBJECT_SUBCLASS |
| List available object subclasses. More... | |
| enum class | OBJECT_TRACKING_STATE |
| Lists the different states of object tracking. More... | |
| enum class | OBJECT_ACTION_STATE |
| Lists the different states of an object's actions. More... | |
| enum class | OBJECT_DETECTION_MODEL |
| Lists available models for the object detection module. More... | |
|
strong |
Lists available object classes.
|
strong |
List available object subclasses.
Given as hint, when using object tracking an object can change of sl.OBJECT_SUBCLASS while keeping the same sl.OBJECT_CLASS (i.e.: frame n: sl.OBJECT_SUBCLASS.MOTORBIKE, frame n+1: sl.OBJECT_SUBCLASS.BICYCLE).
| Enumerator | |
|---|---|
| PERSON | |
| BICYCLE | |
| CAR | |
| MOTORBIKE | |
| BUS | |
| TRUCK | |
| BOAT | |
| BACKPACK | |
| HANDBAG | |
| SUITCASE | |
| BIRD | |
| CAT | |
| DOG | |
| HORSE | |
| SHEEP | |
| COW | |
| CELLPHONE | |
| LAPTOP | |
| BANANA | |
| APPLE | |
| ORANGE | |
| CARROT | |
| PERSON_HEAD | |
| SPORTSBALL | |
|
strong |
Lists the different states of object tracking.
| Enumerator | |
|---|---|
| OFF | The tracking is not yet initialized. |
| OK | The object is tracked. |
| SEARCHING | The object could not be detected in the image and is potentially occluded. |
| TERMINATE | This is the last searching state of the track. |
|
strong |
|
strong |
Lists available models for the object detection module.