Structure containing the results of the object detection module. More...
Data Fields | |
| int | nb_objects |
| Number of detected objects. More... | |
| unsigned long long | timestamp |
| Timestamp corresponding to the frame acquisition. More... | |
| int | is_new |
| Whether object_list has already been retrieved or not. | |
| int | is_tracked |
| Whether both the object tracking and the world orientation has been setup. | |
| enum SL_OBJECT_DETECTION_MODEL | detection_model |
| Current SL_OBJECT_DETECTION_MODEL used. | |
| struct SL_ObjectData | object_list [MAX_NUMBER_OBJECT] |
| Array of detected objects. More... | |
Structure containing the results of the object detection module.
The detected objects are listed in object_list.
| int SL_Objects::nb_objects |
Number of detected objects.
| unsigned long long SL_Objects::timestamp |
Timestamp corresponding to the frame acquisition.
This value is especially useful for the async mode to synchronize the data.
| struct SL_ObjectData SL_Objects::object_list[MAX_NUMBER_OBJECT] |
Array of detected objects.