Structure containing information about the properties of a camera. More...
Data Fields | |
| enum SL_CAMERA_STATE | camera_state |
| State of the camera. More... | |
| int | id |
| Id of the camera. More... | |
| unsigned char | path [512] |
| System path of the camera. | |
| enum SL_MODEL | camera_model |
| Model of the camera. | |
| unsigned int | sn |
| Serial number of the camera. More... | |
| enum SL_INPUT_TYPE | input_type |
| Input type of the camera. | |
Structure containing information about the properties of a camera.
| enum SL_CAMERA_STATE SL_DeviceProperties::camera_state |
State of the camera.
Default: SL_CAMERA_STATE_NOT_AVAILABLE
| int SL_DeviceProperties::id |
Id of the camera.
Default: -1
| unsigned int SL_DeviceProperties::sn |
Serial number of the camera.
Default: 0