Structure containing the results of the body tracking module. More...
Data Fields | |
| int | nb_bodies |
| Number of detected bodies/persons. More... | |
| unsigned long long | timestamp |
| Timestamp corresponding to the frame acquisition. More... | |
| int | is_new |
| Whether body_list has already been retrieved or not. | |
| int | is_tracked |
| Whether both the body tracking and the world orientation has been setup. | |
| enum SL_INFERENCE_PRECISION | inference_precision_mode |
| Status of the actual inference precision mode used to detect the bodies/persons. More... | |
| enum SL_BODY_FORMAT | body_format |
| Body format used in sl::BodyTrackingParameters.body_format parameter. | |
| struct SL_BodyData | body_list [MAX_NUMBER_OBJECT] |
| Array of bodies/persons. More... | |
Structure containing the results of the body tracking module.
The detected bodies/persons are listed in body_list.
| int SL_Bodies::nb_bodies |
Number of detected bodies/persons.
| unsigned long long SL_Bodies::timestamp |
Timestamp corresponding to the frame acquisition.
This value is especially useful for the async mode to synchronize the data.
| enum SL_INFERENCE_PRECISION SL_Bodies::inference_precision_mode |
Status of the actual inference precision mode used to detect the bodies/persons.
| struct SL_BodyData SL_Bodies::body_list[MAX_NUMBER_OBJECT] |
Array of bodies/persons.