Deprecated List
Member Camera::retrieveBodies (Bodies &bodies, BodyTrackingRuntimeParameters parameters, unsigned int instance_id=0)
setBodyTrackingRuntimeParameters and retrieveBodies(Bodies &bodies, const unsigned int instance_id) functions should be used instead
Member Camera::retrieveCustomObjects (Objects &objects, CustomObjectDetectionRuntimeParameters parameters, const unsigned int instance_id=0)
setCustomObjectDetectionRuntimeParameters and retrieveObjects(Objects &objects, const unsigned int instance_id) methods should be used instead
Member Camera::retrieveObjects (Objects &objects, ObjectDetectionRuntimeParameters parameters, const unsigned int instance_id=0)
setObjectDetectionRuntimeParameters and retrieveObjects(Objects &objects, const unsigned int instance_id) methods should be used instead
Member InitParameters::async_image_retrieval
This parameter is deprecated and no longer has any effect.
Member sl::GEN_2
.
Member sl::PERFORMANCE
Computation mode optimized for speed.
Member sl::QUALITY
Computation mode designed for challenging areas with untextured surfaces.
Member sl::ULTRA
Computation mode that favors edges and sharpness.
Requires more GPU memory and computation power.