Classes | |
| class | MODEL |
| Lists ZED camera model. More... | |
| class | INPUT_TYPE |
| Lists available input types in the ZED SDK. More... | |
| class | CAMERA_STATE |
| Lists possible camera states. More... | |
| class | DeviceProperties |
| Class containing information about the properties of a camera. More... | |
| class | SIDE |
| Lists possible sides on which to get data from. More... | |
| class | VIDEO_SETTINGS |
| Lists available camera settings for the camera (contrast, hue, saturation, gain, ...). More... | |
| class | VIEW |
| Lists available views. More... | |
| class | TIME_REFERENCE |
| Lists possible time references for timestamps or data. More... | |
| class | SVO_COMPRESSION_MODE |
| Lists available compression modes for SVO recording. More... | |
| class | MODULE |
| Lists available module. More... | |
| class | FLIP_MODE |
| Lists possible flip modes of the camera. More... | |
| class | BUS_TYPE |
| Lists available LIVE input type in the ZED SDK. More... | |
| class | InputType |
| Class defining the input type used in the ZED SDK. More... | |
| class | InitParameters |
| Class containing the options used to initialize the sl.Camera object. More... | |
| class | STREAMING_CODEC |
| Lists the different encoding types for image streaming. More... | |
| class | StreamingProperties |
| Class containing information about the properties of a streaming device. More... | |
| class | StreamingParameters |
| Class containing the options used to stream with the ZED SDK. More... | |
| class | RecordingParameters |
| Class containing the options used to record. More... | |
| class | HealthStatus |
| Structure containing the self diagnostic results of the image/depth That information can be retrieved by sl::Camera::getHealthStatus(), and enabled by sl::InitParameters::enable_image_validity_check. More... | |
| class | RecordingStatus |
| Class containing information about the status of the recording. More... | |
| class | Camera |
| This class serves as the primary interface between the camera and the various features provided by the SDK. More... | |
| class | InitParametersOne |
| Class containing the options used to initialize the sl.CameraOne object. More... | |
Functions | |
| Resolution | get_resolution (RESOLUTION resolution) |
| Gets the corresponding sl.Resolution from an sl.RESOLUTION. More... | |
| Resolution pyzed.sl.get_resolution | ( | RESOLUTION | resolution | ) |
Gets the corresponding sl.Resolution from an sl.RESOLUTION.
| resolution | : The wanted sl.RESOLUTION. |