Classes | |
| class | AI_MODELS |
| Lists available AI models. More... | |
| class | OBJECT_DETECTION_MODEL |
| Lists available models for the object detection module. More... | |
| class | OBJECT_FILTERING_MODE |
| Lists supported bounding box preprocessing. More... | |
| class | OBJECT_CLASS |
| Lists available object classes. More... | |
| class | OBJECT_SUBCLASS |
| List available object subclasses. More... | |
| class | OBJECT_TRACKING_STATE |
| Lists the different states of object tracking. More... | |
| class | OBJECT_ACTION_STATE |
| Lists the different states of an object's actions. More... | |
| class | ObjectData |
| Class containing data of a detected object such as its bounding_box, label, id and its 3D position. More... | |
| class | CustomBoxObjectData |
| Class that store externally detected objects. More... | |
| class | CustomMaskObjectData |
| Class storing externally detected objects. More... | |
| class | ObjectsBatch |
| Class containing batched data of a detected objects from the object detection module. More... | |
| class | Objects |
| Class containing the results of the object detection module. More... | |
| class | BatchParameters |
| Class containing a set of parameters for batch object detection. More... | |
| class | ObjectDetectionParameters |
| Class containing a set of parameters for the object detection module. More... | |
| class | ObjectDetectionRuntimeParameters |
| Class containing a set of runtime parameters for the object detection module. More... | |
| class | CustomObjectDetectionProperties |
| Class containing a set of runtime properties of a certain class ID for the object detection module using a custom model. More... | |
| class | CustomObjectDetectionRuntimeParameters |
| Class containing a set of runtime parameters for the object detection module using your own model ran by the SDK. More... | |
Functions | |
| def | generate_unique_id () |
| Generate a UUID like unique id to help identify and track AI detections. | |