Fusion Module

Classes

class  COMM_TYPE
 Lists the different types of communications available for Fusion module. More...
 
class  FUSION_ERROR_CODE
 Lists the types of error that can be raised by the Fusion. More...
 
class  SENDER_ERROR_CODE
 Lists the types of error that can be raised during the Fusion by senders. More...
 
class  POSITION_TYPE
 Lists the types of possible position outputs. More...
 
class  CommunicationParameters
 Holds the communication parameter to configure the connection between senders and receiver. More...
 
class  FusionConfiguration
 Useful struct to store the Fusion configuration, can be read from /write to a JSON file. More...
 
class  GNSSCalibrationParameters
 Holds the options used for calibrating GNSS / VIO. More...
 
class  PositionalTrackingFusionParameters
 Holds the options used for initializing the positional tracking fusion module. More...
 
class  BodyTrackingFusionParameters
 Holds the options used to initialize the body tracking module of the Fusion. More...
 
class  BodyTrackingFusionRuntimeParameters
 Holds the options used to change the behavior of the body tracking module at runtime. More...
 
class  CameraMetrics
 Holds the metrics of a sender in the fusion process. More...
 
class  FusionMetrics
 Holds the metrics of the fusion process. More...
 
class  CameraIdentifier
 Used to identify a specific camera in the Fusion API. More...
 
class  ECEF
 Represents a world position in ECEF format. More...
 
class  LatLng
 Represents a world position in LatLng format. More...
 
class  UTM
 Represents a world position in UTM format. More...
 
class  GeoConverter
 Purely static class for Geo functions. More...
 
class  GeoPose
 Holds Geo reference position. More...
 
class  InitFusionParameters
 Holds the options used to initialize the Fusion object. More...
 
class  Fusion
 Holds Fusion process data and functions. More...
 

Functions

FusionConfiguration read_fusion_configuration_file_from_serial (self, str json_config_filename, int serial_number, COORDINATE_SYSTEM coord_system, UNIT unit)
 Read a configuration JSON file to configure a fusion process. More...
 
list[FusionConfiguration] read_fusion_configuration_file (str json_config_filename, COORDINATE_SYSTEM coord_system, UNIT unit)
 Read a Configuration JSON file to configure a fusion process. More...
 
list[FusionConfiguration] read_fusion_configuration_json (dict fusion_configuration, COORDINATE_SYSTEM coord_system, UNIT unit)
 Read a Configuration JSON to configure a fusion process. More...
 
def write_configuration_file (str json_config_filename, list fusion_configurations, COORDINATE_SYSTEM coord_sys, UNIT unit)
 Write a Configuration JSON file to configure a fusion process. More...
 

Function Documentation

◆ read_fusion_configuration_file_from_serial()

FusionConfiguration pyzed.sl.read_fusion_configuration_file_from_serial (   self,
str  json_config_filename,
int  serial_number,
COORDINATE_SYSTEM  coord_system,
UNIT  unit 
)

Read a configuration JSON file to configure a fusion process.

Parameters
json_config_filename: The name of the JSON file containing the configuration.
serial_number: The serial number of the ZED Camera you want to retrieve.
coord_system: The COORDINATE_SYSTEM in which you want the World Pose to be in.
unit: The UNIT in which you want the World Pose to be in.
Returns
A FusionConfiguration for the requested camera.
Note
Empty if no data were found for the requested camera.

Referenced by FusionConfiguration.input_type().

◆ read_fusion_configuration_file()

list[FusionConfiguration] pyzed.sl.read_fusion_configuration_file ( str  json_config_filename,
COORDINATE_SYSTEM  coord_system,
UNIT  unit 
)

Read a Configuration JSON file to configure a fusion process.

Parameters
json_config_filename: The name of the JSON file containing the configuration.
coord_sys: The COORDINATE_SYSTEM in which you want the World Pose to be in.
unit: The UNIT in which you want the World Pose to be in.
Returns
A list of FusionConfiguration for all the camera present in the file.
Note
Empty if no data were found for the requested camera.

Referenced by FusionConfiguration.input_type().

◆ read_fusion_configuration_json()

list[FusionConfiguration] pyzed.sl.read_fusion_configuration_json ( dict  fusion_configuration,
COORDINATE_SYSTEM  coord_system,
UNIT  unit 
)

Read a Configuration JSON to configure a fusion process.

Parameters
fusion_configuration: The JSON containing the configuration.
coord_sys: The COORDINATE_SYSTEM in which you want the World Pose to be in.
unit: The UNIT in which you want the World Pose to be in.
Returns
A list of FusionConfiguration for all the camera present in the file.
Note
Empty if no data were found for the requested camera.

Referenced by FusionConfiguration.input_type().

◆ write_configuration_file()

def pyzed.sl.write_configuration_file ( str  json_config_filename,
list  fusion_configurations,
COORDINATE_SYSTEM  coord_sys,
UNIT  unit 
)

Write a Configuration JSON file to configure a fusion process.

Parameters
json_config_filename: The name of the JSON that will contain the information.
confA list of FusionConfiguration listing all the camera configurations.
coord_sys: The COORDINATE_SYSTEM in which the World Pose is.
unit: The UNIT in which the World Pose is.

Referenced by FusionConfiguration.input_type().