> For clean Markdown of any page, append .md to the page URL.
> For a complete documentation index, see https://docs.stereolabs.com/llms.txt.
> For AI client integration (Claude Code, Cursor, etc.), connect to the MCP server at https://docs.stereolabs.com/_mcp/server.

# Adding Depth Perception in ROS

> **Warning**
>
> **The ZED ROS Wrapper packages are no longer maintained** because ROS 1 reached [end-of-life (EOL) on 2025-05-31](https://www.ros.org/blog/noetic-eol/) with the final Noetic release.
>
> We recommend upgrading to [ROS 2](/docs/integrations/ros-2) to take advantage of the latest ZED SDK features for robotics applications.

## Depth with RViz

In this tutorial, you will learn in detail how to configure your own RViz session to see only the depth data that you require.

Depth information can be visualized in many different ways: 2D depth images, 3D point clouds, 3D registered depth clouds, and the confidence image to name a few.

### Depth image

To visualize a `depth image`, you can use the simple `Image` plugin since the depth data are published on topics of type `sensor_msgs/Image` (see [Video with RViz](/docs/integrations/ros/video-capture/#video-with-rviz)). It differs from a "normal" image in that the data is encoded in 32-bit (floating point) not 8-bit.

![RViz Depth](/_fern-img/82c234cd938ea09050ac15ec90d4f504025208e8ea22f9baa726879516afd66e.webp)

The parameters are the same as for `Image`, with three additions:

* `Normalize range`: Since a floating point image is not directly rendered, it is converted to an 8-bit grayscale image. Enabling this field means the normalization range is automatically calculated
* `Min value`: If `Normalize range` is unchecked, you can manually set the minimum depth range in meters
* `Max value`: If `Normalize range` is unchecked, you can manually set the maximum depth range in meters

Manually setting the normalization range is useful if you know the maximum value measured for the depth and you want to keep the image scale static.

### Depth cloud

The `Depth Cloud` plugin is the first method to visualize the registered point cloud generated by the Depth and Video data streams.
This plugin takes a depth image and an RGB image (both published in the same `frame_id`) and automatically generates a 3D RGB point cloud.

![Depth Cloud](https://cdn.sanity.io/images/s18ewfw4/production/3fda2e17f0e5c3aef6e66043fa6b0e3df04ade34-1836x799.webp)

Key parameters:

* `Depth map topic`: Selects the depth image topic to visualize from the list of available images in the combo box (check `Topic filter` to select only image topics with a name that recalls a depth image)
* `Color image topic`: Selects the RGB image topic to associate with the depth image from the list of available images in the combo box
* `Style`: The style used to render each point. Use `Points` and `Size=1` to maximize FPS
* `Color transformer`: Selects how points are colored. Use `RGB8` to match the color image pixels to the corresponding depth pixels. Use `Axis color` to use a color proportional to the value of the `Axis` value (e.g. `Z` to use a color scale proportional to the distance from the floor or `X` to use a color proportional to the distance from the camera)

### Pointcloud

To directly visualize a topic of type `sensor_msgs/PointCloud2` you can use the `PointCloud2` plugin.

![Point Cloud](https://cdn.sanity.io/images/s18ewfw4/production/c6ef9f1bebf580d1df8e5227da1b81bca3d2f3a0-1836x842.webp)

Key parameters:

* `Topic`: Selects the topic to visualize from the list of available point cloud messages
* `Unreliable`: Check this option to reduce the bandwidth required to subscribe to pointcloud2 topics. The subscriber will use the UDP protocol and will receive messages according to the available bandwidth

You can change the rendering style and the color transformer as explained above for the `Depth Cloud` plugin.

> **Note**
>
> If mapping is enabled (see the `mapping/mapping_enabled` parameter), the `PointCloud2` plugin is also used to visualize the fused point cloud produced by the mapping process, by subscribing to the topic `/zed/zed_node/mapping/fused_cloud`.

### Confidence

To visualize the `Confidence Map` as an image, you can use the `Image` plugin subscribing to the topic `/zed/zed_node/confidence/confidence_map`.

![Confidence](/_fern-img/57a40d5054bf8199034bdd7fd2dec5895c7a98874e5315663b48a133afdd9490.webp)

The confidence values range from 0 (high confidence) to 100 (low confidence): the lighter a pixel, the less reliable its corresponding depth value is.

### Disparity

A plugin for RViz to visualize a disparity message on the topic of type `stereo_msgs/Disparity` is not available, but you can use the `disparity_view` node available in the `image_view` package.

Launch the Disparity Viewer to visualize the disparity image that is published on the topic `/zed/zed_node/disparity/disparity_image`:

```bash
rosrun image_view disparity_view image:=/zed/zed_node/disparity/disparity_image
```

![Disparity](/_fern-img/7919efd76746c71180b3f3b6bd7b74c512187500d8216e654034d484c495c1c5.webp)

## Depth subscribing in C++

In this tutorial, you will learn how to write a simple C++ node that subscribes to messages of type
`sensor_msgs/Image` in order to retrieve depth images published by the ZED node and to get the measured distance at the center of the image.

### Introduction

Use the following command to connect the ZED camera to the ROS network:

* **ZED:**

```bash
roslaunch zed_wrapper zed.launch
```

* **ZED Mini:**

```bash
roslaunch zed_wrapper zedm.launch
```

* **ZED 2:**

```bash
roslaunch zed_wrapper zed2.launch
```

* **ZED 2i:**

```bash
roslaunch zed_wrapper zed2i.launch
```

* **ZED X:**

```bash
roslaunch zed_wrapper zedx.launch
```

* **ZED X Mini:**

```bash
roslaunch zed_wrapper zedxm.launch
```

The ZED node starts to publish depth data to the network only if there is another node that subscribes to the corresponding topic.

> **Note**
>
> The code below subscribes to topics in the `/zed/zed_node` namespace used by `zed.launch`. With the other launch files, the namespace is named after the camera model (for example `/zed2i/zed_node`): change the topic names in the code or remap them when running the node.

### Running the tutorial

If you correctly followed the [ROS Installation Guide](/docs/integrations/ros/#installation), the executable of this tutorial has already been compiled and you can run the subscriber node using this command:

```bash
rosrun zed_depth_sub_tutorial zed_depth_sub
```

If the ZED node is running and a camera is connected or you have loaded an SVO file, you will receive
the following stream of messages confirming that you are correctly subscribing to the ZED image topics:

```bash
[ INFO] [1536333274.037315688]: Center distance : 8.02716 m
[ INFO] [1536333274.069109441]: Center distance : 8.254 m
[ INFO] [1536333274.098305840]: Center distance : 8.56422 m
[ INFO] [1536333274.131910095]: Center distance : 8.69654 m
[ INFO] [1536333274.165769231]: Center distance : 8.82226 m
[ INFO] [1536333274.199659376]: Center distance : 8.9063 m
[ INFO] [1536333274.231564127]: Center distance : 8.92613 m
[ INFO] [1536333274.266022192]: Center distance : 9.02576 m
[ INFO] [1536333274.298987484]: Center distance : 9.19211 m
[ INFO] [1536333274.331713084]: Center distance : 9.09591 m
[ INFO] [1536333274.364827728]: Center distance : 9.0887 m
[ INFO] [1536333274.398832072]: Center distance : 9.07384 m
[ INFO] [1536333274.433348261]: Center distance : 9.27523 m
[ INFO] [1536333274.465598994]: Center distance : 9.10038 m
[ INFO] [1536333274.499350052]: Center distance : 9.10001 m

[...]
```

### The code

The source code of the subscriber node `zed_depth_sub_tutorial.cpp`:

```C
#include <ros/ros.h>
#include <sensor_msgs/Image.h>

/**
 * Subscriber callback
 */
void depthCallback(const sensor_msgs::Image::ConstPtr& msg) {

    // Get a pointer to the depth values casting the data
    // pointer to floating point
    float* depths = (float*)(&msg->data[0]);

    // Image coordinates of the center pixel
    int u = msg->width / 2;
    int v = msg->height / 2;

    // Linear index of the center pixel
    int centerIdx = u + msg->width * v;

    // Output the measure
    ROS_INFO("Center distance : %g m", depths[centerIdx]);
}

/**
 * Node main function
 */
int main(int argc, char** argv) {
    // Node initialization
    ros::init(argc, argv, "zed_depth_subscriber");
    ros::NodeHandle n;

    // Depth topic subscriber
    ros::Subscriber subDepth = n.subscribe("/zed/zed_node/depth/depth_registered", 10,
                                           depthCallback);

    // Node execution
    ros::spin();

    return 0;
}
```

### The code explained

The following is a brief explanation of the source code above.

```C
void depthCallback(const sensor_msgs::Image::ConstPtr& msg) {

    // Get a pointer to the depth values casting the data
    // pointer to floating point
    float* depths = (float*)(&msg->data[0]);

    // Image coordinates of the center pixel
    int u = msg->width / 2;
    int v = msg->height / 2;

    // Linear index of the center pixel
    int centerIdx = u + msg->width * v;

    // Output the measure
    ROS_INFO("Center distance : %g m", depths[centerIdx]);
}
```

This callback is executed when the subscriber node receives a message of type `sensor_msgs/Image` that matches
the subscribed topic `/zed/zed_node/depth/depth_registered`.
The parameter of the callback is a `boost::shared_ptr` to the received message. This means you don't have to worry about memory management.

The callback demonstrates how to access message data:

* The pointer to the `data` field is cast to `float*` because the field is declared as an array of `uint8` values
* The image coordinates \[u,v] of the center of the depth image are calculated
* Since the data are organized in a linear vector, the index of the central pixel is calculated from the image coordinates
* The measure in meters of the center point is printed on the screen

The `main` function is very standard and it is explained in detail in the ["Talker/Listener" ROS tutorial](http://wiki.ros.org/ROS/Tutorials/WritingPublisherSubscriber%28c%2B%2B%29).

The most important lesson of the above code is how the subscribers are defined:

```C
    // Subscribers
    ros::Subscriber subDepth = n.subscribe("/zed/zed_node/depth/depth_registered", 10,
                                           depthCallback);
```

A `ros::Subscriber` is a ROS object that listens to the network and waits for its own topic message to be available.
When a message is received, it executes the callback assigned to it.

In the tutorial, we declared one subscriber to the depth data. The subscriber to the `/zed/zed_node/depth/depth_registered` topic calls the `depthCallback` function when it receives a message of type
`sensor_msgs/Image` that matches that topic.

### Conclusion

The full source code of this tutorial is available on GitHub in the [zed\_depth\_sub\_tutorial](https://github.com/stereolabs/zed-ros-examples/tree/master/tutorials/zed_depth_sub_tutorial) sub-package.
Along with the node source code, you can find the `package.xml` and `CMakeLists.txt` files that complete the tutorial package.