Get Started with ZED Box Orin

Stereolabs’ ZED Box Orin is a compact gateway powered by NVIDIA® Jetson™ for challenging AIoT (Artificial Intelligence of Things) in mobile and field situations. It is designed to bring spatial perception and understanding at the edge and aggregate, process, and analyze data from 3D sensors and equipment.

Options #

The ZED Box Orin provides a set of options that users can choose from based on their specific needs and use cases.

GMSL2 Option #

The GMSL2 option is one of the key features of the ZED Box Orin, which enables high-speed, low-latency data transfer between the processing unit and your ZED GMSL2 cameras, making it an ideal choice for industrial grade applications.

The ZED Box Orin with GMSL2 option is available in three configurations:

To get started with using GMSL2 cameras with your ZED Box, please take a look at our guide Getting started with GMSL2.

📌 * ZED X Driver v1.3.0 or newer required to use more than two GMSL2 cameras with the ZED Box Orin.

📌 * When using the ZED X One 4K, only two of them are supported simultaneously, or one ZED X One 4K together with one Global Shutter model (stereo or monocular), respecting the index rule: the 4K model must always be connected to the lower-ranked port index.

📌 Note: When using 4x cameras on a single 4-wire GMSL2 port, the maximum frame rate is limited to 30 FPS for HD Resolutions or 60 FPS for SVGA resolution.

GPS Option #

With the GPS option, users can take advantage of the ZED Box Orin’s advanced processing capabilities to create AI systems that can operate with high precision and accuracy, even in challenging environments.

You can get started with setting up the GNSS module with our guide Using GNSS with ZED Box. The guide includes step-by-step instructions on how to enable the GNSS module on the ZED Box Orin and configure it for optimal performance.