Telemetry Introduction Access Token Access tokens are the secret passwords that gives access to your resources through the APIs. You can create an API token from the Cloud as described in the introduction. Make sure to keep your tokens secret and to not publish them publicly to prevent any security breach. API in use The Cloud API centralizes all your teams, workspaces, devices, applications, logs and telemetries. hub.stereolabs.com/api/v1 List and query telemetries Get the telemetry from the workspace identified by workspaceId. Multiple parameters are available to customize the output of this endpoint. :workspaceId integer Id of the target workspace. fields string_list optional Telemetry's fields that should be returned by the request. This can be used to reduce amount of data retrieved by only selecting the needed fields. ?fields=timestamp,label,payload Available fields: id, device_id, timestamp, payload, retention, label, tags. Payload fields: A field can also be taken from the payload with the following notation. ?fields=payload.temperature,payload.humidity ids integer_list optional Filter the telemetries from their Id. ?ids=125,356,542 devices integer_list optional Filter telemetries based on the devices that emitted them. ?devices=1,5 labels string_list optional Filter telemetries based on their label. ?labels=detections,environment tags string_list optional Only select telemetries matching all the tags listed. ?tags=main_building startend timestamp optional Only target the telemetry published within the specified the time-range. ?start=1567413071229&end=1567419371229 start and end can be used independently. Timestamps can be provided in the following formats: start=1567419371229 A milliseconds UTC EPOCH UNIX timestamp. start=2019-09-02T11:21:11,229+02:00 An ISO8601 datetime string (must be url-encoded). sortsort_direction field_liststring_list optional Sort the returned telemetry by the specified key. ?sort=timestamp&sort_direction=DESC The order can be specified with the sort_direction parameter that can be DESC or ASC whether you are using descending or ascending sorting. If more than one key is given, the next fields will be used when sorting with the previous key reported an equality. ?sort=label,payload.humidity&sort_direction=ASC,DESC filter_opfilter_fieldfilter_value stringfieldvalue optional Filter out telemetry that doesn't match the specified condition. ?filter_field=payload.temperature&filter_op=gt&filter_value=30 Only return telemetry with a reported temperature over 30° (where temperature is a custom field in the payload). Available filter operations are: gt: is greater than gte: is greater than or equal lt: is lower than lte: is lower than of equal eq: is equal neq: is different contains: is containing the value (string) To avoid type ambiguity when filtering on a payload key, use the filter_value_type parameter and set it to number or string. To use more than one filter, append from _1 to _10 at the end of each filter_* parameter. ?filter_field_2=payload.humidity&filter_op_2=eq&filter_value_2=95 aggagg_fieldagg_step stringfieldtimestamp optional This parameter will change the output format by returning aggregates of telemetry in time-intervals rather than a telemetry list. ?agg=mean&agg_field=payload.temperature&start=1567413071229&end=1567419371229 Returns the average temperature in a time-range (where payload.temperature is a custom field). Available aggregations are: count: Count the number of telemetry matching the provided parameters sum: Sum of the values found in the queried telemetry for the agg_field avg: Average of the values found in the queried telemetry for the agg_field min: Minimum value found in the queried telemetry for the agg_field max: Maximum value found in the queried telemetry for the agg_field If an agg_step is provided, result will be split in multiple time ranges, starting from start and incrementing by agg_step up to the end. An additional agg_identifier can be used to split result in groups based on key's value. ?agg=count&agg_identifier=device_id&start=1567413071229&end=1567419371229&agg_step=36000000 Count the number of telemetry reported by each device in 10 minutes intervals. per_pagepageafter integerinteger_or_fieldvalue optional Controls the pagination of the returned telemetry list. ?per_page=25 By default, the telemetry's timestamp is used to sort the returned page, providing the latest telemetry first. Keyset pagination By using page to select the sorting key, and after to specify the position of the page, pagination will return per_page telemetries starting right after after value ?per_page=25&page=timestamp&after=1567413071229. Offset pagination By using page as a number, pagination will return per_page telemetries starting from the most recent one. ?per_page=25&page=1 limitoffset integerinteger optional Skip some telemetry (offset) and limits the number of telemetry returned by the request. ?offset=50&limit=25 telemetry array List of telemetry matching the specified parameters. /workspaces/:workspaceId/telemetry curl -s \ -H "Content-Type:application/json" \ -H "Authorization:Bearer ${access_token}" \ https://hub.stereolabs.com/api/v1/workspaces/:workspaceId/telemetry \ -G \ -d 'labels=robot' \ -d 'fields=timestamp,payload.temperature' \ -d 'start=1580201472695' \ -d 'filter_field=payload.temperature' \ -d 'filter_op=gt' \ -d 'filter_value=30' HTTP/1.1 200 OK { "telemetry": [ { "timestamp": "1580205472695", "payload": { "temperature":31 } }, { "timestamp": "1580209472695", "payload": { "temperature":45 } }, ... ] } Publish telemetry Publish a new telemetry from the specified device. :workspaceId integer Id of the target workspace. :deviceNameOrId integer Id or url-encoded name of the associated device. label string A string representing the type of telemetry sent. This field is later used during data consultation to filter relevant telemetry. tags string_list optional A comma-separated list of tag to associate with the telemetry. Tags could be used in queries to filter specific telemetries. payload object The actual telemetry data in a json format. This is where you can add custom fields representing your telemetry. timestamp timestamp optional The time at which the telemetry has been generated. Default value is the timestamp at which the request is sent. Timestamp can be provided in the following formats: start=1567419371229 A milliseconds UTC EPOCH UNIX timestamp. start=2019-09-02T11:21:11,229+02:00 An ISO8601 datetime string. (must be url-encoded) retention number optional The retention time of this telemetry in days. If not set, the default value of 1 month (30 days) will be used. id integer ID of the created telemetry. /workspaces/:workspaceId/devices/:deviceNameOrId/telemetry curl -s \ -H "Content-Type:application/json" \ -H "Authorization:Bearer ${access_token}" \ -X POST \ https://hub.stereolabs.com/api/v1/workspaces/:workspaceId/devices/:deviceNameOrId/telemetry \ -d '{ "timestamp": 1567416071229, "label": "people detection", "payload": { "people_count": 54, "accuracy_percent": 98 } }' HTTP/1.1 200 OK { "id": "313233" } Delete telemetry Delete telemetries matching the parameters. :workspaceId integer Id of the target workspace. ids integer_list optional Filter the telemetries from their Id. ?ids=125,356,542 devices integer_list optional Filter telemetries based on the devices that emitted them. ?devices=1,5 labels string_list optional Filter telemetries based on their label. ?labels=detections,environment startend timestamp optional Only target the telemetry published within the specified the time-range. ?start=1567413071229&end=1567419371229 start and end can be used independently. Timestamps can be provided in the following formats: start=1567419371229 A milliseconds UTC EPOCH UNIX timestamp. start=2019-09-02T11:21:11,229+02:00 An ISO8601 datetime string. (must be url-encoded) /workspaces/:workspaceId/telemetry curl -s \ -H "Content-Type:application/json" \ -H "Authorization:Bearer ${access_token}" \ -X DELETE \ https://hub.stereolabs.com/api/v1/workspaces/:workspaceId/telemetry \ -G \ -d 'devices=67890' \ -d 'labels=detections' \ -d 'start=1580201472695' \ -d 'end=1580312563849' HTTP/1.1 200 OK {}