Troubleshooting
This troubleshooting guide provides solutions to common issues that may arise when using the ZED X camera. If you encounter any problems, please refer to the sections below for potential fixes.
The camera is not detected #
GMSL2 cameras have lower flexibility compared to USB cameras. Any modification in the hardware configuration, such as plugging or unplugging a camera, or changing the camera order, requires either rebooting the Jetson, or restarting the installed daemon with the following command:
sudo systemctl restart zed_x_daemon
📌 Note: If you are using a custom carrier board, or a partner’s ECU, please make sure that the custom driver provides the
zed_x_daemonservice. If not, every hardware modification will require a reboot of the Jetson device.
Blurry images after system update #
After a system update, if you experience blurry images from the GMSL2 camera, it may be caused by the overwriting of a patched library used by the ZED Link driver.
To fix this issue, please follow this procedure to manually restore the patched library:
Download the latest ZED Link driver package for your device from the ZED X Drivers download page.
Extract the downloaded
.debpackage and copy the patched library to the correct location:ar x stereolabs-zed<model>_<version>-<deser>-<l4t_version>_arm64.deb tar xvf data.tar.xz sudo cp ./tmp/R<l4t_version>/libnvisppg.so /usr/lib/aarch64-linux-gnu/tegra/libnvisppg.soReplace
stereolabs-zed<model>_<version>-<deser>-<l4t_version>_arm64.debwith the actual filename of the downloaded package.Replace
<l4t_version>with your current L4T version (for example,R36.4.3).Reboot the Jetson device:
sudo reboot
After following these steps, the GMSL2 camera should function correctly with clear images.
Contact Support #
If you are unable to resolve your issue, please reach out to us for further assistance.